Input action: Change Language Permalink

CLIENT-DEPENDENT LANGUAGE

The language can be switched individually for each client. The requirement is that the CODESYS Visualization add-on is installed in at least version 4.7.0.0 and the runtime system in version >= V3.5 SP20. When the visualization is started, it is displayed in the language set in the browser (for example, de or en). This language must be available in the project. If the language is not available, then the default texts are displayed. In version 4.6.0.0 and lower, the language was switched for all clients simultaneously.

LANGUAGE CODE

Use the ISO 639 code (for example, de, en, it, zh-CHS) to name a language which exists in the visualization.

“Language”

Language to which the current visualization client is switched.

Example: ‎en‎

_visu_icon_open_input_assistant.png: The Input Assistant offers all languages available in the project.